AIN#.DEADBAND

Description

AIN#.DEADBAND sets the deadband of the analog input signal.

When AIN#.DEADBANDMODE is set to 0, and the value of the analog input is less than the absolute value of AIN#.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the absolute value of AIN#.DEADBAND, then the analog command will be generated using the scaling specified.

When AIN#.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the absolute value of the deadband. When the input is greater than the absolute value of the deadband, the output is equal to (Input - Deadband) * Scaling.

Below are illustrations of this behavior.

Examples

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range 0 to 12.5
Default Value 0
Data Type Float
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AIN1.DEADBAND

3780h

04h

Signed16

-

1000:1

Read/Write

No

AIN2.DEADBAND

3781h

04h

Signed16

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AIN1.DEADBAND

23150

5A6E

Signed16

Read/Write

-

AIN2.DEADBAND

23151

5A6F

Signed16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.DEADBAND

23150

Float

Read/Write

-

AIN2.DEADBAND

23151

Float

Read/Write

-